1/15/2021 5:36 PM | |
Joined: 2/22/2008 Last visit: 4/25/2025 Posts: 2698 Rating:
|
If the start value always is 0, then you can try the example in attachment. There are more options to create your own scale methode in different ways. The example shows two scalings, with analog amlifier and with arithmetic block. Regards, Scorp AttachmentScaling1.zip (378 Downloads) |
1/15/2021 5:41 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
Here a example from me where you can select one of the three ranges (0-4, 0-6, 0-10) via softkeys.
AttachmentSelect_range_0BA8.Standard.zip (417 Downloads) |
Follow us on