2/2/2009 12:26 PM | |
Posts: 5 Rating:
|
Dear all, i am facing problemrelated to alarm logging in PCS7 V7.0SP1.i have changed time on engineering station.After that alarms which were present before time change didn't acknowledged.New alarms generated get acknowledged easily. But previous alarms didn't acknowledge even though after project deactivation.these alarms shows with cross lines.Please see following attachement. Attachmentos-1.zip (217 Downloads) |
2/2/2009 6:06 PM | |
Posts: 2661 Rating:
|
Hi Sachin, The only solution that I can think of is to retrigger these messages! Only then you can acknowledge them. Also see the following FAQ: PCS 7 V6.0 -- OS Alarm Logging - Message Acknowledgment |
Follow us on