4/5/2018 2:59 PM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello, Yes, that will be the only solution. Unless you have basic panel: You have the following possibility: USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels Best regards, Wizard |
4/5/2018 5:38 PM | |
Joined: 9/21/2012 Last visit: 9/10/2025 Posts: 4708 Rating:
|
This works with Basic panels also, you only need to download a different file from Siemens web site. You can also load the display project from the USB drive, if needed. Then some one who has the original project needs to "download" the HMI to the USB drive. |
3/11/2019 2:51 PM | |
Posts: 10 Rating:
|
Hi Wizard Regarding your last answer . "(You can also load the display project from the USB drive, if needed. Then some one who has the original project needs to "download" the HMI to the USB drive) Does this means that if you download the project files on to the USB that the Operator panel will be able to run in runtime again ? |
3/11/2019 5:01 PM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello Lang Piet, Perhaps this link might help: Best regards, Wizard |
Follow us on