(1)| 6/3/2009 11:17 AM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello drozerce; You can use Prosave to upload the compiled program that is in your OP7. Prosave is available on your Protool or WinCC Flexible installation 9or on the installation CD), or you can download it from the following link: http://support.automation.siemens.com/WW/view/en/8253632 However, as stated, what you will get is a compiled version of the program, you cannot use Protool or WinCC Flexible to open and modify the upload. You can only use this upload to download to an identical OP7 as the one you have installed (replacement in the field of a defective unit). If you have to reprogram something, or move the application to a different type of operator panel, you will have to start again from scratch, I'm afraid. There was too little memory available in the older OPs to allow a download of the whole program; even on the newer, Windows-based panels, the programmer must configure the panel to ensure that a modifiable version of the program is saved on the panel. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/3/2009 11:19 AMEither I will have to learn to type faster, or to write shorrter replies. Quick response, Wizard! At least we confirm each other... |
|
| 6/3/2009 11:45 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello guys, Look at
This info could be helpful if you decide to build new project in Protool. Regards Hristo Mihalev |
This contribution was helpful to
|
|
| 2/17/2015 6:41 PM | |
|
Posts: 3 Rating:
|
Hi! Can you give me correct link please? |
| 4/6/2016 11:09 AM | |
|
Joined: 10/2/2013 Last visit: 11/4/2025 Posts: 1 Rating:
|
Hristo, can you advice me where I can find decoder tool?
|
| 1/26/2021 7:22 AM | |
|
Joined: 10/6/2013 Last visit: 3/9/2025 Posts: 6 Rating:
|
Hi everyone , Where i can to get DecoderProSave.exe??? All links are dead!!! Thanks
|
Follow us on