1/26/2021 3:46 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello deadandan, regarding to your enclosed picture I see by all timers TON the same instance-DB. I recommend to use for each timer the separate instance-DB. In STEP 7 (TIA Portal) you can also use FBs with the language S7-GPAPH. This is better to program the sequence via step by step with delays. See in this case the examples of the FAQ: How do you delay transition of steps as a function of the interlock in STEP 7 (TIA Portal)? Cicero |
1/27/2021 2:36 PM | |
Posts: 13 Rating:
|
Hello Cicero, thank you for your suggestions! Yes, in that example I am using the same instance DB (by the way Multi-instance), but I am bothered about the as I mentioned the memory if I using different DB-s for each Timer. |
1/28/2021 9:49 AM | |
Posts: 13 Rating:
|
It is! |
Last edited by: deadandan at: 01/28/2021 09:49:51 |
|
This contribution was helpful to
1 thankful Users |
Follow us on