(2)| 2/24/2021 11:41 AM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi, You are forgetting one step. The activation file must be sent to Siemens via a Support Request. In return, you will get a release file within one day. The release file must be used to activate the additional PO. In the attachment, the release file is missing, so I assume that has not happened yet. You need to use PC where the AS is connected to. In the following link you can find the manual and the procedure on how to update the CPU: |
Last edited by: Oreca at: 02/24/2021 11:44:59Last edited by: Jen_Moderator at: 02/25/2021 07:52:52Optimized link. If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on