(3)| 2/25/2019 10:17 AM | |
|
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
Greeting, Can anybody share the PLC/HMI example program of G120 CU230P-2 DP including VFD Alarms. |
|
MS |
|
| 2/25/2019 11:00 AM | |
|
Joined: 10/11/2006 Last visit: 1/19/2026 Posts: 6069 Rating:
|
Hello, Siemens offers in SIOS a lot of example descriptions / projects for connecting a drive to a PLC. Depending on how you want to control the axis and which PLC you have you should find at least an example which is quite close to your configuration. For example here to control a G120 speed controlled at a S7-1200 via DP: https://support.industry.siemens.com/cs/ww/en/view/70155469 By default you will get the standard system diagnostics with the Profidrive fault classes. If you want to have all warnings and faults with texts you need to download the XML list of the warnings (can be found in the firmware download page of the drive) and use the XML parser to convert the XML data to CSV, which can be imported to TIA Portal then. Here the link to the parser: https://support.industry.siemens.com/cs/ww/en/view/77467239 |
|
With best regards, |
|
This contribution was helpful to
|
|
| 2/27/2019 9:07 AM | |
|
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
Thank You! Yes, It's like a EPOS because following hardware was installed in previous old control system. Old Drive System 1. Lenze Drive 8200 Vector E82EV371_2B with Profibus using PAR +PZD(2Wrote) in HW attached. 2. Danfoss Bauer BS02-34H gear motor n1-1350/min n2-127/min 50Hz 3. THALHEIM Baumer ATD3B B14 Y13 12 PB encoder with Profibus using PNO Class 2 16Bit resolution 1Word in HW attached. 4. CPU 315 PN/DP with box PC 620 using SIMATIC V5 New Drive System 1. G120 CU230P-2 DP 2. Existing Motors 3. Existing Encoders with Profibus 4. CPU 314C PN/DP with KTP900 using TIA V15 In this scenario is following examples can be used for CU230P-2 DP with connectivity of Profibus encoder to directly CPU. Is MC_Home is suitable for this encoder application and EPOS blocks for CU230P-2 DP OR any other Library blocks in your Opinion. MC power block not available in TIA library for CPU314C & CU230P-2 DP. AttachmentHW Config.zip (284 Downloads) |
Last edited by: Sarfraz Bashir at: 2/27/2019 9:15:52 AMLast edited by: Sarfraz Bashir at: 2/27/2019 9:21:04 AMLast edited by: Jen_Moderator at: 2/27/2019 12:20:08 PMOptimized links. MS |
|
This contribution was helpful to
|
|
| 2/28/2019 12:37 PM | |
|
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
Thank You! Team, There is one Software-based solution for position-controlled tasks. Easy Motion Control (TIA Portal)Applications include approaching absolute positions or relative traversing, as well as simple gearbox synchronism, both with linear and rotary axes. Easy Motion Control is the obvious choice when 1 to 5 axes per machine are to be traversed Free choice of drives (except stepper motors) Different interface modules can be used for encoder acquisition and set point output, depending on the application. Input drivers for position acquisition for CPU 314C PROFIBUS DP absolute encoder Universal drivers for any interface modules Output drivers for controlling the drive for CPU 314C MICROMASTER 4 over PROFIBUS DP Universal driver Is it suitable solution for attached Device & Network...?? |
Last edited by: MS1981 at: 2/28/2019 12:38:28 PMMS |
|
| 3/3/2021 3:48 PM | |
|
Joined: 1/1/2017 Last visit: 10/30/2025 Posts: 343 Rating:
|
Thank you very much! Regards OmKris |
Follow us on