10/17/2016 12:09 PM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating:
|
Hi to al In reference of my last help posted on Logo Support: Multiple LOGO on HMI Panel I have to resolve how to connect 31 LOGO!s network project to ONE connection HMI PKT700 Basic panel. On Logo! Soft Confort V.8.0 Im able to configure the network of one HMI panel + 31 Logo's ( this is the limits) See in attachment the project test connection. As said before, on my WinCC basic are working only 4 Connections, this 4 connection im able to set the IP address to 4 LOGO!s You write that in LOGO network project i can integrating max 32 LOGO ( as my project demo) for a total of 128 LOGO!s 32 Logo network X 4 connection= 128 LOGO!s, is correct? In the theory this 32 LOGO!s network project I have to connect ALL in ONE winCC Connection, but there I'm NOT able to connect or find how to configure this 32 LOGO!s in one connection. Please can someone make me a winCC project example how to connect 31 LOGO!s network on one WinCC connection port? Thanks again for the help Attachment31 Logo to HMI Network.zip (227 Downloads) |
10/17/2016 2:06 PM | |
Joined: 12/18/2014 Last visit: 9/3/2025 Posts: 35917 Rating:
|
FS4 is a new firmware. LOGO! can not upgrade or downgrade the Firmware. You must buy a new LOGO! FS4. |
Follow us on