7/2/2013 5:24 PM | |
Posts: 25 Rating:
|
here is were i am...at this very moment(attachement) |
7/2/2013 5:37 PM | |
Posts: 25 Rating:
|
the thing is i am using an ethernet connection to comuniate from the pc to plc and i d-nt have a mpi cable so i need to use unly the ethernet(343-1) |
7/2/2013 5:55 PM | |
Posts: 25 Rating:
|
yes i have a 317-2dp and a 343-1...and i am using the second one to connect to the first via ethernet |
7/2/2013 7:46 PM | |
Posts: 25 Rating:
|
yes,,,,thank you this is my plc program without hmi...
Attachmentscoala.zip (210 Downloads) |