10/10/2016 12:06 PM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating:
|
Hello, someone can help me to reply on this question? It is possible to use up to 220 logo8 on network? thanks |
10/17/2016 11:20 AM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating:
|
Hi, please last help for clarify all.. On Logo! Soft Confort V.8.0 Im able to configure the network of one HMI panel + 31 Logo's ( this is the limits) See in attachment the project test connection. As you said before, on my WinCC basic are working only 4 Connections, this 4 connection im able to set the IP address to 4 LOGO!s You write that in LOGO network project i can integrating max 32 LOGO ( as my project demo) for a total of 128 LOGO!s 32 Logo network X 4 connection= 128 LOGO!s, correct? In the theory this 32 LOGO!s network project I have to connect ALL in ONE winCC Connection, but there I'm NOT able to connect or find how to configure this 32 LOGO!s in one connection. Please can someone make me a winCC project example how to connect 31 LOGO!s network on one WinCC connection port? Thanks again Attachment31 Logo to HMI Network.zip (342 Downloads) |
10/17/2016 11:44 AM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating:
|
ok thanks again Where I can post this issue for getting WinCC support? |
10/17/2016 11:58 AM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
A new topic for WinCC (TIA Portal) you can make here: https://support.industry.siemens.com/tf/de/en/threads/261/?page=0&pageSize=10 Describe exactly which panel you want to use and which software version. Basic or other. |
Follow us on