4/9/2017 8:31 PM | |
Joined: 4/28/2015 Last visit: 3/12/2025 Posts: 578 Rating:
|
The SDK of the example image does not come with kernel headers. Would have to be enable explicitly during the build. See also http://stackoverflow.com/questions/31256770/using-populate-sdk-to-include-kernel-headers. According to github, it seems you are already trying to rebuild the image from source, which is the cleaner way in any case: add a recipe to build your module during the image generation. |
This contribution was helpful to
1 thankful Users |
4/15/2017 1:28 PM | |
Joined: 2/14/2017 Last visit: 4/17/2023 Posts: 59 Rating:
|
Now that I can successfully build the example image from source, I will try this. I am unsure about the following:
I'm not sure what the correct config file is in the IOT2000 Example Image to do that
|
5/6/2017 5:51 PM | |
Joined: 2/14/2017 Last visit: 4/17/2023 Posts: 59 Rating:
|
I still don't have the headers in /usr/src after this exercise. Help is welcome. |
Follow us on