7/12/2022 9:35 AM | |
Joined: 4/28/2020 Last visit: 9/2/2025 Posts: 30 Rating:
|
Thanks. So, now, I have a length that I can give in myself ( in cm), and an analog value that's converted to a speed in cm/min. Is there a way to make a constant calculation of the remaining length? So: the length that I gave in should be constantly reduce, dependent on the speed (analog value). Purpose is to unroll a coil with fiber at a certain speed (analog value) and to know when the coil will be empty. In best case, we can constantly see the remaining length on the coil. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 07/12/2022 15:37:56New subject after splitting |
|
7/12/2022 3:42 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
Here an example.
AttachmentConstant_calculation_of_the_remaining_length_0BA8.Standard.zip (856 Downloads) |
This contribution was helpful to
1 thankful Users |
7/12/2022 3:57 PM | |
Joined: 4/28/2020 Last visit: 9/2/2025 Posts: 30 Rating:
|
Thanks a lot! I'll try to understand that now :D |
7/13/2022 9:54 AM | |
Joined: 4/28/2020 Last visit: 9/2/2025 Posts: 30 Rating:
|
Thanks for that! Now I made the program myself, but seems like there's still something wrong. When I enable the I1, to start the cyclus, it doesn't start from the given value (here 10000) but it starts reducing from 0. Any idea what I do wrong? Thanks in advance AttachmentLeegloopdetectie_2.zip (951 Downloads) |
7/13/2022 1:21 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
That is the problem by LOGO!. The LOGO! can only calculate with integer values. |
Follow us on