9/16/2015 1:32 AM | |
Posts: 23 Rating:
|
is it not possible to program in STL or in ladder logic. |
9/16/2015 8:52 AM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
But please remember, that SCL is a fee-based option. If you do not have SCL, you have to use STL and. indirect addressing, even if it is more laborious. Agreed ,But the initiator should tell us what programming options are available for him/her SET |
This contribution was helpful to
2 thankful Users |
10/1/2015 6:25 AM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
one more query i want to sort the DB values from Low to High or High to low, for all three DB's in which value is stored.Is there any function in S7-300 PLC library which help in sorting. For sorting values in a DB, you can try the function explained in the following FAQ.Just additional point to be considered, to keep consistency of the logging data, copy the original data to a Sorting DB and perform sorting on that. Sample program for sorting a data block |
10/3/2015 11:13 PM | |
Posts: 23 Rating:
|
Dear, Please see the program, I am not getting same values after sorting. in DB2 Initially i keep value in DB2 and then give M0.2=true |
Follow us on