8/10/2009 10:41 PM | |
Posts: 2661 Rating:
|
Hi olu, Have a look at the following FAQ: How can you generate user-defined operator input messages in WinCC? Regards |
8/11/2009 10:45 PM | |
Posts: 2661 Rating:
|
Can you explain what you mean by this? Check if the following help: How can you create operator inputs through user-specific actions in up to and including WinCC V6.0 SP4? |
Last edited by: Phantom75 at: 8/12/2009 12:14 AM |
|
8/12/2009 11:45 PM | |
Posts: 2661 Rating:
|
Can you copy the valve parameter windowto a test PDL and post in forum? |
8/14/2009 5:56 AM | |
Posts: 21 Rating:
|
Please find herewith attached Test.pdl Regards, Olu AttachmentTest.zip (521 Downloads) |
This contribution was helpful to
1 thankful Users |
8/14/2009 10:15 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi use this script to get the old and the new value of the IOField for the Event-text (Variable MsgEvent)of the message: char *oldVal, *newVal, MsgEvent[255]; oldVal = GetPropChar(lpszPictureName,lpszObjectName,"OutputValue"); newVal = GetPropChar(lpszPictureName,lpszObjectName,"InputValue"); sprintf (MsgEvent,"%s changed: new: %s old: %s", lpszObjectName,newVal, oldVal); trigger the script by "event" > "Output/Input" > "Input Value" > "Change" use this to create the message How can you generate user-defined operator input messages in WinCC? regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
8/14/2009 12:53 PM | |
Posts: 21 Rating:
|
Hello cumulus, thanks for your reply, I tried this however Old and New Value in Messageare same which is New Value. Regards, olu |
Follow us on