6/21/2019 8:29 PM | |
Posts: 11 Rating:
|
Hello! I was checking this topic to know how to solve an alarm I'm having at this time: 230001 Axis B1 SERVO_3:3:5(5) Component Motor_module_11: Power unit: Overcurrent: Fault cause: 11 bin As I saw in this post the problem was overcurrent on bin 10 (V phase), and my problem is bin 11, is this W phase, Am I wrong? Can you help me with it or I need to make another topic? Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/24/2019 12:24:29New subject after splitting |
|
6/28/2019 5:29 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, It is not double channel. It is single chanel. [0] = motor encoder feedback & [1] = external encoder feedback. You need to activate motor encoder feed back, de activate safety integrated & reference the axis. Then check the difference between motor & encoder position. Then set safety integrated. For more detailes, please refer SINUMERIK 840D sl Commissioning CNC: NC, PLC, Drive , SINUMERIK 840D sl/SINAMICS S120, SINUMERIK Safety Integrated , SINUMERIK 840D sl Safety Integrated HTH |
Last edited by: Jen_Moderator at: 07/04/2019 15:05:02Optimized links. |
|