3/20/2013 1:11 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, The manual “SIMATIC S7-1500 Structure and Use of the CPU Memory”( http://support.automation.siemens.com/BR/view/en/59193101) on Chapter 3.2.4 Shows a sample project for Data Log. AttachmentData logging.zip (1517 Downloads) |
Last edited by: O_Moderator at: 3/20/2013 1:20 PMLast edited by: Pegaia at: 3/20/2013 1:13 PMDenilson Pegaia |
|
This contribution was helpful to
3 thankful Users |
8/19/2013 12:31 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi petr1234, Witch block / command did you use? |
Denilson Pegaia |
|
3/13/2014 2:06 PM | |
Posts: 5 Rating:
|
Hello,
AttachmentEnergy_measurement_BDNNN.zip (727 Downloads) |
3/26/2014 11:08 AM | |
Posts: 10 Rating:
|
HI BDNNN It will not let me upload the file. All i did was add a number to the name string using the concat function. and i incremented the number when needed and the problem was solved. i did try to send. Regards Cowmanator
|
3/27/2014 2:57 PM | |
Posts: 5 Rating:
|
Hello Cowmanator, I succesfully used the concat block. But I have some troubles converting the number (INT) to a string. I use the S_CONV block. the result is a string of the int with some spaces before the number. And the datalogcreate block doesnt accept names with spaces in :/ Your project might be helpful. Did you try to archive your project and then zip it (winzip)? It should be possible to upload the zipfile. Kind regards, Bruno |
4/28/2014 4:29 PM | |
Posts: 5 Rating:
|
Hello, Thank you for your help! It works now :) Kind regards, Bruno |
4/24/2015 8:22 AM | |
Posts: 7 Rating:
|
Hello Pegaia, Many thanx for your program, it helped me a lot! For now I have 1 question left, how many records can I assign to the 'DataLogCreate' block? The 'Records' tag is a UDint, that means more then 4 billion. But when I assign more then 32000 records the block just dont execute when I put an logic 1 on the REQ input. I also dont give an error nor status (7000).
|
11/11/2015 5:59 PM | |
Posts: 1 Rating:
|
Hello Denilson, I have TIA Portal V13. And I can not open the sample program of data logging. Could you send that suitable for V13? Thank you. |
3/31/2019 10:25 AM | |
Joined: 5/22/2016 Last visit: 10/18/2023 Posts: 2 Rating:
|
I Have used your program to create a Datalog in TIA V15 and PLCSIM ADVANCED V2. It works fine, becouse I can see in monitoring Datalogocreate, 1 number of done and a increased number in monitoring Datalogwrite. But I can see the file datalog through the webserver. Do you have any clue? |
Last edited by: josejack at: 3/31/2019 10:27:50 AM |
|
Follow us on