8/25/2020 3:37 PM | |
Joined: 5/7/2013 Last visit: 12/13/2024 Posts: 42 Rating:
|
everything works, I was a victim of my multi screen and resolution arrangement (the drop down appeared but tiny on another screen) my goal is to set the timer for a wiping relay via the ouput of a multiplexer (see attachment), it works principally but if the longer time (60) is stil running and I set the new time (15) the relay is reset; can that be avoided somehow ? I know there are a few alternative ways to do it but this would be very elegant ------------------------------------------------------------------------------------------ AttachmentSchaltplan2.zip (351 Downloads) |
Last edited by: Jen_Moderator at: 09/02/2020 11:55:08New subject after splitting |
|
9/1/2020 2:14 PM | |
Joined: 5/7/2013 Last visit: 12/13/2024 Posts: 42 Rating:
|
somehow those functionalities do not like me... I want to use the output of a counter as the timer input for a wiping relay, if I do that the max. time base selectable is minutes, for fixed values hours are possible also. How come ? I attach a simple example BR George AttachmentSchaltplan2.zip (369 Downloads) |
9/2/2020 11:07 AM | |
Joined: 12/18/2014 Last visit: 9/11/2025 Posts: 35950 Rating:
|
It's like you may or may not believe me. Or start a Support Request, then you will get an official answer from Siemens.
|
Follow us on