1/30/2016 12:13 AM | |
Posts: 76 Rating:
|
Hi all I have a problem with simotion d425 , run is ok but the led of ready is red evertime, the machine was worked and the suddenly, I dont cant information about the fault, the device diagnostic: Event id 16# F364:B284 Also the segment display show 6. and point is flash Attach diagnostic device thanks in advance Attachmentdsaig.txt (855 Downloads) |
2/1/2016 6:16 PM | |
Posts: 76 Rating:
|
Thanks for response . Yes I made the device diagnost, and upload now and also the screenshott AttachmentDevice Diagnostics_sim D425.rar (789 Downloads) |
Last edited by: mnada at: 2/1/2016 6:21:56 PM |
|
2/1/2016 6:24 PM | |
Posts: 76 Rating:
|
and screnshoot
AttachmentDibujo.rar (703 Downloads) |
2/2/2016 6:53 AM | |
Posts: 1529 Rating:
|
And please show the diagnostics buffer. |
2/2/2016 10:12 PM | |
Posts: 76 Rating:
|
Up load new diagnost, I think when analyze the buffer ,the number 6 point is when change for not ready I wait some response, thanks in advance AttachmentL_Stacker.rar (580 Downloads) |
2/4/2016 10:45 PM | |
Posts: 76 Rating:
|
Hi all, first to all thanks for the advices Hi had problem with the target network of me laptop, and I didnt see, dont work well , I changed and install socut 4.3.1 in other laptop and go online for ethernet, very nice, go online very well, and I find the fault when go online with sinamics integrated, witch show fault 30xxx , motor ground or wire motor wrong, I2t, I check and is well , but the drive was wrong , I changed drive, and change the topology as well the amount power in dirve ( that is more big that the was replaced, drive old 5A , new drive 9A), and recognoce the topology, all fault was up, I dont have fault, and I can move the servo from simotion in control panel, but I think some part of programme is lost , due to dont move when the machine ask, so now I waiting for the original programm for up load and charge in the simotion or need to doing another thing , reset factory from sinamics integrated?, upload buffer after and before from replace drive AttachmentDevice Diagnostics_04_01_2016.txt (553 Downloads) |
Follow us on