1/7/2018 7:29 PM | |
Posts: 200 Rating:
|
Taking the example from a previous post the value that is given i would like to change from the HMI i have use a simple I/O display on the screen which is replicating the figure that the Logo is giving out, in the HMI i can press on the value and it allows me to enter a figure bit when i press enter it goes bach to figure in the Logo and docent change hope this makes sense i can send some screen shots in the morning thanks AttachmentPressure.lsc.zip (392 Downloads) |
This contribution was helpful to
1 thankful Users |