3/30/2021 11:57 PM | |
Joined: 8/12/2015 Last visit: 5/29/2025 Posts: 2 Rating:
|
Network speed is 12Mpbs , but I have tried all speeds without any results. All addresses are unique and I have tried different address to the problematic node. PLC has address 2 , and the node with the problem is 10 (but have tried multiple addresses) the other nodes are 11,12,13. Prosoft module that has the problem supports DPV1 and DPV0 , but the vendor of the device says we should only use it as DPV0 and this is what we have configure it to. The vendor claims that when we go online to the PLC , we potentially send DPV1 messages that the can't reply. This is not confirmed because they have not run diagnostics on the prosoft yet. The rest of the PB nodes are always healthy , no matter the network settings. TIA connects to PLC through X2 on Ethernet. Cabling is ok, we have tested temp cables, different plugs etc. Attachmentprosoft.zip (349 Downloads) |
Follow us on