4/27/2021 10:14 AM | |
Posts: 5 Rating:
|
Hi, i have a similar problem... i´m trying to comunicate via profibus a kuka robot with a S7-1200 (CM1242-5) via profibus. my configuration doesn´t work. I configure a profibus connection and area transfer in the cm1242-5... the led DIAG is switch off and the led of RUN/STOP is in amber, the PLC diagnosis show me the next message: existing module. faulty. led error(SF). can somebody help me? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/27/2021 12:09:04New subject after splitting |
|
4/27/2021 3:09 PM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, yes, then cooperate with that CM module documentation where is desciption about cfg and other useful infos. You need cfg some I/O buffer where data can be exchanged (robot). You can also look here for little other tip: Topic: Use S7-1200 as PB Slave to DCS |
Last edited by: Duris_I at: 04/27/2021 15:18:40With best regards... |
|
Follow us on