7/5/2021 4:05 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello BigBanq; When you upload from a S7-300 PLC, you can only recuperate what was loaded on the PLC originally, so you can get the code. But unfortunately the comments, the symbols and the gsd files are not loaded to the PLC with the program, so you cannot locate them. Since you modified the uploaded program and then downloaded it again to the PLC, you overwrote the existing program and the parameters for the non-Siemens gsd files are missing. The gsd files for Siemens automation are included in Step 7, so these will not give you a problem. You will therefore need to locate these 3rd-party gsd files, integrate them in Step 7 and parameterize them for this application. Here is what is possible to find for the 3 files you pointed out: - D2V_V20C.GSD: This file cannot be located under that name, can you provide us with the make and model of the Profibus slave? - TR06AAAB.GSE: The manual for the TR electronics encoder can be found here, it includes a download path for the gsd file. https://www.tr-electronic.com/f/TR-ECE-BA-GB-0028 - BC3150.GSD: http://www.gsd-db.com/view.php?gsd=bc31074b.gsg You musy register in the gsd-db site to download this file, or you can look for it on the Beckhoff website. https://infosys.beckhoff.com/english.php?content=../content/1033/bx3100/3238548747.html&id= Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 07/05/2021 16:16:13 |
|
7/5/2021 5:19 PM | |
Posts: 5 Rating:
|
Another picture of it. Thanks. |
7/5/2021 5:37 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello BigBanq; Thank you for the information and photographs provided. Unfortunately, even now all i can find is this pdf describng the Profibus slave, not the gsd itelf: https://www.konecranes.com/sites/default/files/download/dynavectorii.pdf DynABus II > Profibus-DP field bus > Data frame based on Profidrive PPO5 specification, which is completed for crane applications > Crane terminology and wide status information > Full crane control features > Possibility for redundant signals via Profibus and terminals Since the responsability for developping and distributing the gsd file for Profibus/Profinet equipment is on the manufacturer, I can only suggest you contact Konecranes.com and ask their support techs to provide this file to you. Hope this helps, Daniel Chartier |
Follow us on