8/7/2021 7:38 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, High overload & low overload depends upon motor loading or application load cycle. User can check connected motor Kw & can work. e.g. if connected motor is 11 KW rating, then application demand is high overload where as connected motor capacity is 15 Kw rating then application demand is low overload. Please refer attached sheet for more details. (extracted from Siemens manual) P.S. - Please check p0205 value i.e. inverter application. 0 = high overload 1 = low overload AttachmentCONVERTER OVERLOAD CAPACITY.pdf (682 Downloads) |
Last edited by: PISCEAN 2010 at: 08/07/2021 07:57:01P. S. added Last edited by: PISCEAN 2010 at: 08/07/2021 08:10:22 |
|
This contribution was helpful to
1 thankful Users |
Follow us on