8/16/2021 10:30 PM | |
Joined: 1/30/2021 Last visit: 11/11/2023 Posts: 1 Rating:
|
Poderia me ajudar? com qual versão do step 7 voçe consegue comunicar com a maquina? Porque precisei fazer upload e não consegui. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/17/2021 09:45:23New subject after splitting |
|
8/17/2021 9:48 AM | |
Joined: 5/12/2006 Last visit: 9/18/2025 Posts: 22710 Rating:
|
step7 V5.x and Sinumerik Toolbox |
8/17/2021 10:11 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello vicentibarbosa, Which is the controller? If it is 840D SL you will need Simatic Manager Step 7 v 5.6. With LAN cable you can establish communication & upload PLC station. If you have 840D PL, you will need Simatic Manager Step 7 v 5.4. If you have PG you can establish communication via MPI port with MPI cable & can upload PLC station. If you don't have MPI port you will need 6GK1571-1AA00 MPI USB adaptor to establish communication. HTH |
Follow us on