8/22/2021 6:30 PM | |
Joined: 9/27/2006 Last visit: 9/17/2025 Posts: 12411 Rating:
|
Hello is_razi; I believe this doument should answer your question, and put your mind at ease: - SINAMICS Power Modules PM240-2/PM240P-2/SINAMICS G120C/SINAMICS G120X: Advantages of the integrated DC link reactor https://support.industry.siemens.com/cs/ww/en/view/109749021 So for G120 and G120x drives of the appropriate frame sizes( above 15 kW) there is an integrated DC inductabce in the circuit, so that there is no need to purchace an external AC line reactor. Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
8/23/2021 6:06 AM | |
Joined: 3/13/2009 Last visit: 7/12/2025 Posts: 132 Rating:
|
Sure it does , Thanks for your very enlightening explanation. |
Follow us on