8/27/2021 9:03 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Yes you can use it as 1phase 200-240V AC input & 200-240V 3 phase AC output. Please refer attached datasheet. Attachment6SL3210-1PB13-0UL0_datasheet_en.pdf (530 Downloads) |
This contribution was helpful to
1 thankful Users |
8/30/2021 6:13 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hello, Don't forget that in addition to the power module part number you have quoted, you also require a control unit to control said power unit. See HERE to view the available control units, it largely depends on what your application is, as there are control units specifically for pumps and fans (CU230P-2 DP or PN), some general purpose (CU240E-2 DP or PN) and some with encoder interfaces (CU250S-2 DP or PN) to list a few examples. Regards, Graeme |
Follow us on