8/31/2021 10:55 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello mburnett01, the AI module 6ES7134-6GD01-0BA1 is compatible for the ET 200SP prozessor and the reason could be the firmware of the ET 200 SP CPU. Check the firmware version of the ET 200SP and if possible make the update. Use the link for the download: Firmware update S7-1500 CPUs incl. Displays and ET 200 CPUs (ET 200SP, ET 200pro) Have you standardize and destandardize the analog values with STEP 7 (TIA Portal)? Compile the project complete with the both instructions
And download the program again. With best regards |
Follow us on