6/28/2019 9:48 AM | |
Posts: 5 Rating:
|
Hello, members of this tread We have basically the similar problem mentioned above.
When we try to change the SW logic for controling the drive (just for testing purpose), means first we set the signal for traversing and than set the enable bit, it works well and no alarm appear. But this is not solution for me (cannot change the customer standard blocks). These things drive me crazy, any idea what to do or check next?
------------------------------------------------------------------------------------------ Attachmentdoc1.pdf (389 Downloads) |
Last edited by: The Helping Hand at: 06/28/2019 11:40:53New subject after splitting |
|
6/28/2019 10:33 AM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, < Firmware Version 4.7 HF11 no alarm 7496 occurs. With Firmware Version 4.7 HF11 this is fixed, and if position controller is not enabled 7496 occurs. In general: It is helpful to use SinaPos for controlling Basic Positioner. https://support.industry.siemens.com/cs/ww/en/view/109736845 |
With best regards, |
|
Follow us on