9/1/2021 4:35 PM | |
Joined: 7/13/2020 Last visit: 1/12/2024 Posts: 11 Rating:
|
Hello! I am working on a PLC panel consisting of the following: ET200SP Standalone PLC (6ES7510-1DJ01-0AB0) HMI (6AV2123-2DB03-0AX0) Aswell as I/O modules: DI, DQ, AI, AQ. I was wondering about the correct way to protect my PLC, HMI and I/O potential group. I want to protect these but I'm not sure what size fuses to get. I.e the PLC has a current rating of 0.9A but an inrush current of 4,7A. What size circuit breaker should I get for it? and is it necessary to use one or can I wire the PLC directly from the supply? FYI the PLC panel will only be used for learning purposes and not actually in the fields.. but I still want to make a good panel. Thanks for any insight! |
Last edited by: aleksPLCSIM at: 09/01/2021 16:36:10Last edited by: The Helping Hand at: 09/02/2021 09:42:43Optimized links. |
|
9/11/2021 1:12 PM | |
Joined: 7/13/2020 Last visit: 1/12/2024 Posts: 11 Rating:
|
Here are the 4 units: 4XL 2/4 wire ST 6es7134 6gd01 0BA1 6es7 131-6bf01 0ba0 di 8x24VDC ST Thanks for any insight! |
Follow us on