10/7/2021 9:51 AM | |
Joined: 7/5/2018 Last visit: 8/28/2025 Posts: 19 Rating:
|
Hello RafaVidal, Please send a screenshot of the error shown. mui94 |
This contribution was helpful to
1 thankful Users |
10/8/2021 9:22 AM | |
Joined: 7/5/2018 Last visit: 8/28/2025 Posts: 19 Rating:
|
Hello Rafa, about the message that appears referring to the memory, even if it is not completely full, when you load your device, the equipment requires part of this memory to perform an internal compilation and then load the program itself. If the CPU does not have space in its memory for this compilation, this message appears. This is usually solved if you safely remove the memory card and with the help of a Field PG load the project directly onto it. As for the web server problem, I would recommend that you contact Siemens Technical Support. mui94 |
This contribution was helpful to
1 thankful Users |
10/8/2021 10:14 AM | |
Joined: 8/14/2021 Last visit: 10/23/2024 Posts: 17 Rating:
|
Thanks Mui94, and sorry for send my message in spanish. Thanks. |
Follow us on