10/31/2021 5:56 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, 6ES7153-2AA02-0XB0 is a too old module. It's obsolete as well. its release date from 1999. And it can accommodate up to 8 modules (ET200M). Its successor 6ES7153-2BA02-0XB0 can accommodate up to 12 modules (ET200M). Both modules can work together with the same CPU in different racks without any conflict. But in the case of redundancy (using RED Bundle), you have to use the same MLFB with the same FW for both IM modules in each rack. |
Ayman Elotaify |
|
Follow us on