11/4/2021 5:39 PM | |
Joined: 9/14/2016 Last visit: 7/18/2025 Posts: 34 Rating:
|
Hello, I have the same problem. I'm using: ET200 CM Ptp 6ES7137-6AA01-0BA0. There is no Hardware Address in that area. No %I4.0, no %IB4, no %IW4, no %ID4 up to address 50, while the CM Ptp uses only a few bytes I moved all my addresses above 50, and yet the PLC gives this error. The only way it seems to go away is by making the CM Ptp put it's data starting from address 4 or by changing the hardware module to 6ES7137-6AA00-0BA0 (only in the project). But neither of this solves the actual problem: Modbus over RS485 on 2 wires does not work. Led on TX blinks but no actual data is transmitted over it. (our team looked it up over osciloscope). Modbus RTU blocks are V3. Later versions are not compatible for some reason. Version 2 gives the same result. Modbus Master gives back response timeout error as if the partner is not responding. (which is legit since no data is transmitted to slave) We even changed the ET200 PLC and the CM Ptp with new ones. Partner of Modbus was changed as well, but he is fine we checked Modbus RTU (on RS485 2 wire mode) on it with a s7-1200 and works just fine. Firmware used on ET200 PLC is 2.9, and TIA Portal V17. All hardware settings of CM Ptp are set as we always used it for 2 wire mode for the Older version of CM Ptp. Wiring was done on pin 12 and 14, as we always have done for previous modules for 2 wire mode. We also changed wires between pins 12 and 14 with the same result, (sometimes RS485 is manufactured with inverted polarity on the behalf of partner). For some reason the HW_ID is no longer showing up... in TIA Portal V17. I only found it in the Tags section at constants. We recently migrated to V17 for this exact problem as according to datasheet ET200 CM Ptp 6ES7137-6AA01-0BA0 is available only from TIA V17 or newer. Maybe I'm missing something. Any help is much appreciated. Regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/05/2021 09:11:15New subject after splitting |
|
Follow us on