11/26/2021 12:00 PM | |
Joined: 11/6/2020 Last visit: 7/29/2025 Posts: 14 Rating:
|
Hello, I have a similar problem. I configured an array of UDT's inside a UDT. (Alarmlimit in the picture is part of an UDT). I tried to connect this UDT to the interface of my faceplate, that causes the error (pasted below). Is it even possible to add an array in an interface? Interface tags[0]: Position_Comm - The data type 'Array [0..5] of F2_UDT_SENSOR_SETTING_ALARMLIMIET' of member 'Settings.Alarmlimit' in 'F2_UDT_SENSOR_COMM V 0.0.1' is not supported. Select a supported data type. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/26/2021 13:29:01New subject after splitting |
|
Follow us on