10/22/2014 1:49 PM | |
Posts: 2 Rating:
|
I have only serial connection to my drive. My comoputer have not serial port and I use a converter USB/Serial.The configurations used are in attached file. Impossible to make connection to drive. For USB/serial converter I installed the drive delivered by producer on the CD exactlly for my OS - Windows 7 Professional - 64 bits.
AttachmentUSB_SERIAL.pdf (643 Downloads) |
12/17/2021 4:53 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello varunbudde, User can provide external 24 V DC supply to CU240S, terminal 31 +24V DC & terminal 32 0Volt. Advantage of doing so is, even if PM supply is OFF, CU can be in network & status can be seen. Hope this helps. |
Follow us on