3/16/2022 9:22 AM | |
Joined: 9/2/2021 Last visit: 7/3/2025 Posts: 5 Rating:
|
Dear experts, I have several G120c inverters in each project which takes a lot of time to commission. I would like to have a quick way to set the motor parameters. With the EditParametersInSeveralDrivesAddIn I tried this but get some errors and parameters aren't changed in the project. The parameter list comes from a saved user-defined parameter list from an existing drive. I added the log file in the attachment. Do you have tips to solve this problem or another program to help me? AttachmentEditParametersInSeveralDrivesAddIn Log_1532022_1413.txt (390 Downloads) |
Follow us on