5/30/2022 4:47 PM | |
Joined: 6/4/2010 Last visit: 9/30/2024 Posts: 387 Rating:
|
Dear Mattias, The replacement of the Desigo SX-Open is the Desigo Connect. This is the logical migration path. Desigo CC™ Connect is a gateway between systems with different protocols. Desigo CC™ Connect as a software platform, incorporates the industry’s latest software technology to integrate BACnet, Modbus, KNX, M-bus, SNMP, S7 and various disciplines (for example, Danger Management), into a common object model and is supported by a powerful computational engine. For further information please see:https://sid.siemens.com/go/A6V11852735 Unfortunately there is no automated workflow or Excel Macro to migrate the SX-OPC configuration to Desigo CC - OPC csv file. Please note that the Desigo CC -Wrapper is not supported anymore and there is SIOS article on it Somebody who knows SX-OPC configuration and Desigo CC – OPC csv can manually and efficiently migrate the integration. Best regards, Albis |
This contribution was helpful to
1 thankful Users |
Follow us on