6/2/2023 10:00 AM | |
Joined: 12/18/2020 Last visit: 8/7/2025 Posts: 23 Rating:
|
Hello, The WinCC Unified PC Runtime V18 - Update 1 - Service Release 2 is not the solution to these error. It can be only a TIA Portal V18 (WinCC Unified ES V18) update or SR. I contact this morning the hotline, and this problem was send to Germany in the factory. I Will return you if any reply.
|
6/2/2023 10:17 AM | |
Joined: 1/21/2013 Last visit: 9/9/2025 Posts: 4099 Rating:
|
Hi JD2Grenoble, The ability to dynamize the alarm control filter was removed in V18. I don't know if this was done intentionally or by accident, but you're not the first to complain about it. As far as I know, it was supposed to be reinstated in V19. But instead of waiting for V19, you can use the scripting elsewhere. For example, you can use Screen.Items to access the alarm control from anywhere on the screen, or you can use a dynamizable property and access the alarm control using the item parameter. Then use the Filter property to change the filter. Kind regards |
This contribution was helpful to
1 thankful Users |
6/2/2023 10:29 AM | |
Joined: 12/18/2020 Last visit: 8/7/2025 Posts: 23 Rating:
|
Hi, Arcuarius. I hope it will reinstated in V18 UP2, and this update came before end of July. Javascript is not so easy for me. I start with COM TEXT, and Protools.. I've 57 y.o. I use 4 hours on a sunday to write and test my script, and now I should to more test again ? I will try to found help about Item parameter on youtube. Thanks a lot.
|
Follow us on