6/14/2023 12:58 PM | |
Joined: 1/21/2013 Last visit: 9/18/2025 Posts: 4111 Rating:
|
Hi JobKaptein, Please refer to the "External Tags" chapter in the "WinCC Engineering V18 - WinCC Unified" system manual. There you will find the following information: All simple data types available on the connected PLC are available at an external tag in WinCC. … Interconnected PLC data types and arrays are not supported. Only the S7-1500 communication channel supports user defined data types. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on