11/14/2022 2:45 PM | |
Joined: 8/7/2020 Last visit: 5/29/2025 Posts: 12 Rating:
|
Hello fel low programmers! I use Wincc unified PC Runtime V17 update 4 on ITP1000 tablet. I'm asking for help with one of my issues. I configured an alarm log with parameters seen in attachment. On one of my screens I use alarm control where alarm source is set to Logged alarms. The option Show recent is also checked. The log works fine until it reaches 1000 rows. I know that this is the maximum that the alarm control can show and that's fine. The problem is that recent logged alarms are not shown anymore. I have to upload the whole project again and tick the option Reset all logs in runtime everytime that the number of rows reaches 1000. I want the alarm control window to always show recent 1000 logged alarms. I don't know if my problem is with alarm log configuration or with my alarm control settings. Any help would be greatly appriciated! Best regards Attachment2022-11-14 15_34_57-Siemens - C__Users_filipk_Documents_Automation_PTL010_PTL010.png (714 Downloads) |
11/15/2022 6:32 PM | |
Joined: 8/6/2018 Last visit: 9/3/2025 Posts: 366 Rating:
|
Hello, Have you tried update 5? It brings improvements in the behaviour of the alarms. Thanks you |
Follow us on