7/28/2024 1:22 PM | |
Posts: 1 Rating:
|
Dear Sir, First time I am here in this forum. I need some technical advice regarding G120 drive. Previously, we were using Micromaster 440, 30kW 6SE6440-2UD33 with input and output reactors.And it also has a break resistance 15 ohm, 2200 W. We need to upgrade to G120 (6SL3210-1PE26-0UL0). for new module, It is mentioned that this power module G120, has built in Break Resistance. And also I looked in power module, didn't find any terminals to connect break resistance with it. And what about input and output reactors. Shall I use for new drive module also which were used for old MM440 (SIE 6SE64004BD222EA0) Kindly advice me so I can start commissioning for this new G120. Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/01/2024 14:26:31New subject after splitting |
|
Follow us on