9/21/2024 11:29 AM | |
Joined: 7/13/2021 Last visit: 1/31/2025 Posts: 4 Rating:
|
hello, i'm facing same problem of HMI KTP700 Basic. Screen Tapping is not working.. *Showing Alarm system - Change to operating mode 'online' which is already online in connection of HMI. - Connection to PLC is established and values can be read and PLC alarms also showing. - Tried Running HMI with Mouse HMI is working. - Done HMI factory reset - Before I was using TIA portal + WinCC V17 and HMI v15.1 in software also updated firmware version and panel images to V17 as i'm using TIA portal + WinCC V17. "Only the issue is Screen taping of HMI is not working and showing Alarm "Change operating mode online " Please help, Is there HMI hardware issue or is there any other solution over this?" ------------------------------------------------------------------------------------------ |
Last edited by: DAKSHAKRAJ at: 09/21/2024 11:34:46Last edited by: Moderator_Lan at: 09/23/2024 07:16:07New subject after splitting |
|
9/23/2024 11:35 AM | |
Joined: 8/3/2009 Last visit: 9/4/2025 Posts: 16343 Rating:
|
Hello DAKSHAKRAJ If the ouch does not work on the Panel (also not if runtime is not running) and you have done a reset to factory settings does not clear the behaviour then I think your display is damaged. In this case: https://support.industry.siemens.com/cs/de/en/view/22639376 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on