11/15/2024 10:57 AM | |
Joined: 2/17/2020 Last visit: 8/29/2025 Posts: 1251 Rating:
|
Hi, Make sure to start the server project in the WinCC Client via the SIMATIC Shell command "Interconnect". This FAQ may also help: Update the configuration file of the WinCC project (delete DCF) |
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
11/17/2024 4:12 AM | |
Posts: 2 Rating:
|
Thanks |
11/19/2024 3:19 PM | |
Joined: 8/3/2009 Last visit: 9/8/2025 Posts: 16353 Rating:
|
Hello Check exactly these FAQs for setting up the all WinCC Stations correctly: https://support.industry.siemens.com/cs/ww/en/view/22132850 https://support.industry.siemens.com/cs/de/en/view/868014 this could also cause such a behaviour if not all settings are correctly Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on