11/27/2024 4:43 PM | |
Joined: 5/12/2022 Last visit: 8/11/2025 Posts: 3 Rating:
|
I currently have an mbNET router (platform mbConnect24) to establish a VPN with a SCADA installation of Siemens WinCC Unified v19 update 3, on a Windows PC. We have created a Web2Go access on the mbConnect24 platform, but when we start HTTPS access we get to the main page of the WinCC Unified Runtime webserver but we cannot go any further. For example we cannot get to the page "Start your project". We get a page error that you can see in the attached file. ( ERR_TOO_MANY_REDIRECTS ) However, when tried to connect using VPN with mbConnect24 using the IP address it's connecting successfully! So, it looks that the problem is in direct access through internet published link because VPN it's almost same as local network I tried to solve the problem with the help of this link, but it doesn't work. How to configure the Siemens WinCC Unified Runtime for use with the HTTP WebAccess Please kindly advice how to configure WinCC Unified for web access??.
|
11/28/2024 7:10 AM | |
Joined: 11/13/2018 Last visit: 8/28/2025 Posts: 91 Rating:
|
Hello Rafa Linares, You talk about Talk2M in the title of your post. I got a WinCC Unified PC Runtime V19 Update 3 working in M2Web. It's important that you add the certificate of the Runtime to your eWon. The steps are explained here. |
Like it? Rate it! |
|
Follow us on