12/5/2024 10:39 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi T_Ebrahem, To be honest, I have no idea how to do this with the old WinCC Comfort Panel. For the WinCC Unified Comfort Panel, however, you can make a backup remotely. This is usually done via TIA Portal or SIMATIC ProSave. Another option is to perform the backup on the device itself and store the result on an external storage medium. And if you are using a system memory card, you can make an automatic backup to this card. FTP is not supported by a WinCC Unified Comfort Panel, although it may be available in the depths of the Debian-based operating system. So you will probably need your own software to perform an automatic remote backup. This may be possible using the SIMATIC Automation Tool SDK. However, you should be aware that a backup will only be possible if the runtime is stopped. To be honest, since you have not yet purchased any hardware, I would recommend that you contact the technical consulting with your requirements. Kind regards |
This contribution was helpful to
2 thankful Users |
12/5/2024 1:48 PM | |
Joined: 1/2/2017 Last visit: 1/17/2025 Posts: 288 Rating:
|
Hi Stefan, Thanks for the informative answer, I have created a support request because we want to be sure before ordering any hardware. Kind regards Ebrahem |
Disclaimer: While I strive to ensure that the content of posts and answers is accurate and complete, my posts and answers are provided “as is” and “as available.” Your use of my posts and answers content is entirely at your own risk. |
|
Follow us on