12/12/2024 12:57 PM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi Venkat2210, In this case, if I understand correctly what you want to do, I understand that it is possible to archive process data into a centrally located SQL Server database using the WinCC Unified platform, even when the SQL Server and WinCC Unified are installed on separate PCs. For database-based archiving, you need the "WinCC Unified Database Storage" option for WinCC Unified PC. This option allows you to store all archive data in an MS SQL server after installing the option and the license ("WinCC Unified Database Storage") You can connect WinCC Unified PC Runtime to a Microsoft SQL database using a "Connection String" or a "File DSN". The connection string contains all necessary information to establish a connection between the runtime and the database ("WinCC Unified: Use of SQLite or Microsoft SQL databases") For remote access, you need to configure the ODBC Data Source on the PC where WinCC Unified Runtime is installed ("How do you archive tags and messages in an SQL database with WinCC (TIA Portal) Advanced?") I believe that with this information you can have valuable information that can help you. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on