12/10/2024 3:51 PM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello HaMi-CS! The error you mention may be caused by an incompatibility. You can check this in the Compability tool, of which I leave you the link and FAQ for help. When it is stated that it is not unlocked/not compatible, it means that the system has not been tested by the Siemens software development department. This implies the very possible occurrence of failures since we can neither predict nor guarantee the operation in such an environment. I hope that is not the cause of the failure, but at least to rule out that option. - https://support.industry.siemens.com/cs/ww/en/view/64847781 |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on