12/13/2024 11:26 AM | |
Joined: 10/22/2012 Last visit: 6/20/2025 Posts: 5 Rating:
|
Hi all, Cross Reference GUI lets you select project objects on the left side and displays usage of these objects within other project objects. This works fine for tags (process variables) and pictures (PDL). But it seems not to work for CScript standard or project functions. I have read a lot of threads pointing to the standard header to include in CScripts that CrossRef can find tag and picture references inside CSripts. This feature already works great for me. What I want to see is, where standard or project functions are called. As an example, I created a trivial project with - single project function calling two standard functions (01) - single start picture with a buttons OnClick event calling the project function and standard functions (02 -03) But selecting the used functions in the CrossRef shows no usage (10,11). Do I expect too much or am I doing something wrong? AttachmentExampleScreenShots.zip (118 Downloads) |
Follow us on