1/16/2025 10:51 AM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16287 Rating:
|
Hello termolar You can see this also in "live" if you connect online to the S71200 and open in TIA Portal the view of the communication ressources in the online view. then you can see how much communication ressources are still free or if you where on max limit. you can check also if perhaps a larger S71200 can do the job You can have also a look at this FAQ: https://support.industry.siemens.com/cs/de/en/view/98699910 (WincC Prof RT acts almost the same as a WinCC V7/8) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on