8/25/2018 8:14 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Detail more information about the problem would help forum member to analyse the problem & help you in better way. Here e.g. is this new machine under commissioning or new running machine? How & when this problem occured? i.e. when switching ON the power after weekly off day or while machine was running? Does operator or any body tried to communicate with NCU? etc. etc. A snap shot of NCU status & OP screen will help much better. Do you have bootable USB drive? You may boot from it to analyse the problem in detail. BTW please find attached file, refer it & compare the various status of LED & 7 segmenet display of your machine. Hope this will help you analyse the problem. Attachment840D SL 7 segment booting display status.pdf (2193 Downloads) |
12/1/2022 9:53 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by AutoGen_3968829 is split to a separate thread with the subject NCU is showing a number 8 on the 7 segment display. Best regards |
This contribution was helpful to
1 thankful Users |
1/17/2025 9:10 AM | |
Joined: 9/17/2024 Last visit: 5/16/2025 Posts: 2 Rating:
|
no answer to this error published? |
1/20/2025 9:12 AM | |
Joined: 7/30/2024 Last visit: 9/10/2025 Posts: 960 Rating:
|
Closed because a new topic is discussing the same issue: 840D SL, 7 segment flashing 3-3-4-6
Kind regards, Moderator_Lan |
Follow us on