1/22/2025 7:56 PM | |
Joined: 11/23/2007 Last visit: 7/10/2025 Posts: 133 Rating:
|
Hi Denilson, Your little example programs are always a source of inspiration. In wincc comfort / advance there is a curve tool (fx from memory) that allows you to display a table of values located in the PLC. This was simple because it was managed with specific bits. With Wincc Pro (TIA) it was necessary to go through a fairly understandable script but tedious when it was necessary to display 20 curves simultaneously. With Unified I do not understand how to do it. Do you have an example? I suspect that it is necessary to go through a script but I do not understand how to do it to - Display my curves with only 1 trigger bit - Have a reactive control (each curve contains 1000 points / values) - My curves are refreshed every 3s approximately. Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 01/23/2025 07:55:51New subject after splitting |
|
Follow us on